PTT是脉搏波传播时间(Pulse Transmit Time)的缩写,指的是同一个周期ECG信号的R波顶点和PPG信号波谷的间隔时间,可以用来进行无创血压的测量,并且相比于充气式血压计,被测者的舒适度更高。由于PTT需要同时对ECG信号和PPG信号进行测量,所以可以使用MAX86150,能同时测量PPG信号和ECG信号,从而方便地计算出PTT。
视图:
Keywords: ECG,PTT,PPG,血压
PTT是脉搏波传播时间(Pulse Transmit Time)的缩写,指的是同一个周期ECG信号的R波顶点和PPG信号波谷的间隔时间,可以用来进行无创血压的测量,并且相比于充气式血压计,被测者的舒适度更高。由于PTT需要同时对ECG信号和PPG信号进行测量,所以可以使用MAX86150,能同时测量PPG信号和ECG信号,从而方便地计算出PTT。