Views:

Question

Part: 104898-HMC394LP4 and HMC705LP4
 
Customer is asking for:
My signal is around 100 MHz +/- 200 kHz. Can it still divide the signal
appropriately ? Also as far as I understand, I can choose the factor of
division from 2-32, meaning I can divide also with a factor of 10 with
this device ? I have the same question about HMC705LP4
 
Answer
 

Yes , can use  HMC394LP4 and HMC705LP4 for 100MHz input. 200 kHz offset does not matter here because this is only 0.2% compare to 100MHz.

HMC394LP4 can divide input frequency to   2,3,4,5…10.32.     

HMC705LP4  can divide input frequency to   1,2,3 …10… 17.