Question
Answer
(1) It may appear that the plugin install is not the updated one. The updated one can be found in the Plug In manager in ACE . Its called Board ADAQ776XIIO.
(2) They will need to use the Plug In Manager in ACE to uninstall Board.ADAQ776X and instead installed Board.ADAQ776XIIO"
(3) The procedure is to uninstalling the board ADAQ776X and Installing the board ADAQ776XIIO the Zedboard will find the correct the plugin and will able to start the evaluation of the hardware.
(4) If you received a SD card with the eval board? It should be able to use that with the plugin, the plugin will configure the SD card. If not, you will need to a SD card of16GB and flash it, by following these instructions as in the link here ADI Kuiper Linux for Evaluation [Analog Devices Wiki]