Views:
Yes.  There is a Visual Basic for Applications example that performs a 1-Wire Search and prints out the ROM numbers of all 1-Wire devices connected on a PC.  The code is embedded in an Excel Spreadsheet.
 
Interested software developers can find the code at this GitHub software repository
 
The pre-requisite to use the spreadsheet is to download and install the 1-Wire Drivers package.  Also, an appropriate 1-Wire PC adapter will need to be connected to the PC after the 1-Wire Drivers package gets installed.   Here is a screenshot of the VBA code running inside an Excel spreadsheet:
 
 
Here is the Search Window populated with discovered 1-Wire devices: