Views:

According to the MAX30102 datasheet, the maximum I2C clock rate is 400KHz. They do not support clock rate at 1Mhz. However, the MAX30102 and MAX30101 have a maximum sampling rate of 3200sps; when reading data under burst mode, the effective data write/read speed is 9600 per second, which is 9.6kHz, so 400kHz is sufficient for the component.

Related Products: MAX30102EFD+
Comments (0)